Automation package for rising stem valves.
 
 

 
Position feedback for single-seat and double-seat valves.
  • Sensor, adapter and actuating element: all in one set.
  • Reliable fixing even in case of strong vibration in the plant.
  • 80 mm stroke monitoring with 3 programmable switching outputs.
  • Switch-point programming via teach pushbuttons and LED feedback.
Installation
This set contains all that is required for automating a rising stem valve. The items supplied cover the rising stem valve sensor, adapter and the actuating element of stainless steel. Quick installation of the adapter and easy switch point teaching by pressing a pushbutton on the sensor reduce the set-up time.

Resistant to vibration
As a result of the optimum distribution of force at the interface from the sensor to the adapter and the adapter-actuator transition this system is insensitive to mechanical stress such as vibration.

Application
Limit detection of hydraulic oils, coolants, water and hydrous media.

ZZ0214 - Rising stem valve sensor

For further information please refer to the current bulletin (pdf file 385 kB).