Due to maintenance work, we are currently unable to provide you with all shop functions.
You probably do not come from: United Arab Emirates. If necessary, change to:United States
  1. New products
  2. Sensors
  3. Chemically resistant capacitive sensors

Chemically resistant capacitive sensors

Perfect switch point setting

The new capacitive sensors impress with their outstanding technical data and the innovative, patented ifm visualisation concept. The sensor’s LED bar display enables the ideal adjustment of the switch point to the application conditions. The switch point is always in the centre of the display, green LEDs on both sides indicate the reliability. Deposits and material changes are directly visible so that the switch point can be easily and precisely readjusted using a potentiometer or IO-Link.

Chemically resistant

The robust and chemically resistant PP housing is specially designed to last in areas with acids and alkalis. This makes the sensor particularly durable and reliable, even in demanding industrial environments, and it is typically used in the semiconductor, solar and chemical industries.

Avoid production downtimes

The IO-Link process value provides information about installation and possible deposits, increases production safety and prevents downtime, which saves costs and ensures smooth operation.

The risk of failures or shutdowns is minimised by detecting and avoiding impending faults in good time. The intuitive LED display facilitates process adjustments and enables simple switch point adjustments by the user.