Due to maintenance work, we are currently unable to provide you with all shop functions.
You probably do not come from: United Arab Emirates. If necessary, change to:United States
  1. New products
  2. Sensors
  3. Hand-held device for an easy location of leaks

Hand-held device for an easy location of leaks

Rapid location of detected leaks

The hand-held device for the location of leaks is an ideal complement for the sensor-based monitoring of the compressed air system. Firstly, data analysis can be used to detect the leak and confine it to a certain area. Then the hand-held device is employed. It can rapidly and easily identify, measure and document the leak from a loss of just 0.1 litres per minute.

Transparency over the cost of leaks at one glance

The SDL100 is equipped with 30 ultrasonic microphones, laser distance measurement, camera and a 3.5-inch display. The microphones detect leaking sounds even at high ambient noise levels. The inaudible ultrasound is converted and delivered as an acoustic signal to the headphones. What is more, the leak is visualised in the live camera image on the display. The ongoing compressed air loss and its cost incurred are displayed, too.

Simplified reporting according to ISO 50001

On site, all information about the leak and its maintenance can be digitally recorded on the SDL100 and then transferred to the free software using a data stick. This simplifies reporting according to ISO 50001.

How to: SDL100 Leak Detector / Hardware

How to: SDL100 Leak Detector / Software