• Products
  • Industries
  • IIoT & Solutions
  • Service
  • Company

Innovation Award of the German Gas Industry 2020

18/2/21

ifm sensors successfully support Graforce in the implementation of climate-neutral improvement concepts.

​Graforce won first place in the German Gas Industry Innovation Award 2020 in the category of efficient energy concepts.
In the image video for the company's innovation award, an exciting find can be made out.

But what are the activities of Graforce and what does ifm have to do with it?

Graforce is involved in the extensive field of hydrogen production and wastewater purification. The company won the German Gas Industry Innovation Award 2020 with its project for completely climate-neutral heating of a hotel building. Currently, Graforce is pursuing the project of climate-neutral wastewater treatment in the Berlin water operation of the Waßmannsdorf sewage treatment plant. Click here for more information on Graforce.

The ifm sensor technology has so far been used in the areas of treatment, exhaust air and water.

Once again, ifm can successfully provide support in the implementation of climate-neutral improvement concepts. At this point, congratulations to Graforce on the excellent placement and here's to continued successful cooperation.