John Deere – How John Deere is digitising its production with IO-Link solutions
Video report
IO-Link masters and sensors as well as connecting data by Bluetooth are the solutions that allows John Deere to use 100% of the advantages of IO-Link. These advantages are the digitalisation of electrical signals and easy setting and diagnostics with the sensors. But also other sensors are used to produce diesel engines for off road applications - such as inductive sensors, sensors with RFID technology, laser sensors as well as pressure and flow measurement sensors. A future project will be the implementation of vibration analysis to monitor electro spindles.