The lower part of the module is simply clicked into the DIN rail.
Lay the two AS-i cables in the recess.
Attach the upper part of the module, turn the locking lever. Ready!
No matter how the flat cable runs, the AS-i ClassicLine module always cuts a fine figure thanks to the rotatable cable guide.
Addressing made easy with the built-in connection for the ifm addressing device (optional).