The compact transmitter with 0.2% accuracy is ideal for sanitary applications.
Explore the features using the interactive model above.
Explore the features using the interactive model above.
Most resilient measurement technology on the market
Especially when compared to thin metal diaphragms, the capacitive ceramic cell is resistant to dents and dings that cause measurement offsets.
Especially when compared to thin metal diaphragms, the capacitive ceramic cell is resistant to dents and dings that cause measurement offsets.
Ingress protection
We’ve eliminated terminal chambers that corrode, removable caps that expose electronics and large housings which collect humid air that condenses inside the sensor.
We’ve eliminated terminal chambers that corrode, removable caps that expose electronics and large housings which collect humid air that condenses inside the sensor.
Optimized vent design
The location of the vent moves it out of the path of overflowing media to avoid clogging. The orientation of the vent can be rotated around the housing to further protect it.
The location of the vent moves it out of the path of overflowing media to avoid clogging. The orientation of the vent can be rotated around the housing to further protect it.
Robust signal transmission
The sensor communicates analog or digital process values over standard M12 cordsets, eliminating the need to wire to terminal blocks, saving installation time, and reducing failures due to corrosion.
The sensor communicates analog or digital process values over standard M12 cordsets, eliminating the need to wire to terminal blocks, saving installation time, and reducing failures due to corrosion.
Process adapters
We offer several process adapters to match the profile of the installed weld-in shell.
We offer several process adapters to match the profile of the installed weld-in shell.
Streamlined profile
The only part of the sensor that is exposed outside the coupling nut is the M12 connection and the atmospheric vent. This leaves the sensor electronics protected inside the weld-in shell and streamlines the sensor profile in the application.
The only part of the sensor that is exposed outside the coupling nut is the M12 connection and the atmospheric vent. This leaves the sensor electronics protected inside the weld-in shell and streamlines the sensor profile in the application.