• Products
  • Industries
  • IIoT & Solutions
  • Supply Chain Software
  • Service
  • Company

When quality is a matter of millimetres

Automotive industry
Body-in-white
Monitoring and maintenance
Product quality
Case Study

How ifm’s PMD Profiler ensures quality in car body manufacturing

Resistant to extraneous
light up to 20,000 lux

Flexible, distance-independent
object positioning

Quick set-up
No expert knowledge needed

Results

  • The PMD Profiler detects missing mats on body parts
  • Resistant to extraneous light and easy to position
  • Simple set-up in just a few minutes, no expert knowledge required
  • Improved quality – costs savings through lower scrap levels
  • High process reliability, no false alarms due to deviations of the object position

The challenge

There is a simple principle in quality control: The sooner errors are discovered, the better. Errors discovered late usually lead to higher costs and more rejects.

At our customer’s body-in-white facility, a 1.3 mm rivet mat is manually glued to a body part in order to reduce noise inside the vehicle. If the mat is missing, the noise level in the car is too high – a no-go for a premium man­ufacturer. If the error is not discovered until later in the process, e.g. in the paint shop, the scrap rate will be considerable.

Quality control of this manual step proved dif­ficult in the past. Because the mat is so thin, measurement with diffuse lasers can be unreli­able. Errors were sometimes not discovered or false alarms were triggered. In addition, checking the correct orientation of the mat is not possi­ble with this approach. Quality assurance with conventional 2D image processing was also ruled out due to the extraneous light in the production hall reducing the detection reliability.

Our customer

As one of Germany’s premium carmakers, our customer has a long and successful history based on a strong tradition of performance and innovation. The brand’s road-approved sports cars combine tradi­tion, design, performance and exclusivity. And of course, discerning customers of premium vehicles expect superior quality.

With electromobility and environmental concerns transforming the automotive industry, improving resource efficiency in the use of raw materials and components also plays a key role in manufacturing. This is why high scrap rates are constant­ly reduced. To achieve this, our customer decided to rely on the experience of ifm.

Our customer

As one of Germany’s premium carmakers, our customer has a long and successful history based on a strong tradition of performance and innovation. The brand’s road-approved sports cars combine tradi­tion, design, performance and exclusivity. And of course, discerning customers of premium vehicles expect superior quality.

With electromobility and environmental concerns transforming the automotive industry, improving resource efficiency in the use of raw materials and components also plays a key role in manufacturing. This is why high scrap rates are constant­ly reduced. To achieve this, our customer decided to rely on the experience of ifm.

The solution – why ifm?

The premium car manufacturer already uses var­ious photoelectric sensors from ifm at their facil­ity. However, many conventional sensors are not suited for this particular application, as a high immunity to extraneous light is required. In addi­tion, the body part and the rivet mat hardly differ in colour and do not offer sufficient contrast for some methods.

The carmaker now uses the PMD Profiler from ifm that works by means of triangulation. The sensor projects a straight laser line onto the body part with the applied rivet mat. The laser light is reflected and detected by the sensor’s receiv­ing element. There is an angular offset between the projection unit and the receiving element, so that the contour sensor can detect an object’s height profile.

Particularly helpful in this application: The pro­portions of the recorded height profile are independent from the distance between the sensor and the object. This makes positioning, installation and configuration of the sensor very easy. Neither external illumination nor screening against extraneous light is required. Reference objects can be taught via three pushbuttons and the intuitive menu navigation of the colour dis­play.

After set-up of the PMD Profiler, an LED indicates whether the current part is OK. Via IO-Link, a digital signal can be transmitted to the PLC for direct processing. With the PMD Profiler, missing rivet mats are now immediately detected, and the body part can be fed back into the manu­al process. This solution prevents rejects due to missing or misapplied mats and allows our cus­tomer to reduce subsequent costs.

Case Study: When quality is a matter of millimetres

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.