• Products
  • Industries
  • IIoT & Solutions
  • Supply Chain Software
  • Service
  • Company

Digital communication to the sensor

  • Volumetric flow and temperature are transmitted as process values, reducing the number of measuring points required
  • Constant and high resolution across the entire measuring range
  • Decentralised IO-Link masters reduce the amount of cabling required
  • Seamless digital documentation
  • Sensor data can be used in an IIoT context

moneo: The IIoT platform

  • Parameter setting
  • Condition monitoring
  • Communication from OT to IT

Possible output functions

Some SV display versions have dual analogue outputs (4...20 mA). This means that the sensors can be easily connected to existing controllers featuring only analogue input cards. Alternatively, the frequency output can be used.

Convert resistance signals

The all-plastic SV version transmits the flow rate via a 4...20 mA signal. The PT1000 signal used to output the temperature can be quickly and easily converted into a 4...20 mA signal using the TP adapter. So the SV transmitter devices can easily function as dual analogue devices and be integrated into existing system or control structures.