Radar sensor for open and closed containers
Precise measurement on open and closed tanks and
containers
The LW2160 radar level sensor measures levels of liquid media up to 10 metres precisely and without blind areas. The 80 GHz technology used ensures stable and precise measurement results, even in the presence of steam or condensate in the tank for example.
With the antenna extension, available as an accessory, the sensor may also be used outside closed metal tanks, for example on open tubs.
The radar measuring system can also penetrate through non-metallic walls, allowing the level sensor to be easily mounted above plastic tanks such as IBC containers.