- New products
- Sensors
- Precise & convenient: radar level sensor with IO-Link
Precise & convenient: radar level sensor with IO-Link

Trouble-free monitoring of large tanks
With the LW2760 level sensor, levels of liquid media in tanks with a height of up to 10 metres can be monitored precisely and without blind areas. The non-contact radar measuring principle prevents malfunctions or failures of the sensor caused by the adhesion of viscous media or damage from agitators.
The 80 GHz technology used ensures stable and precise measurement results even in the presence of steam or condensate in the tank. The sensor is designed for use in hygienic areas, so that even CIP and SIP processes or the use of spray balls do not impair its proper functioning.
More convenience thanks to IO-Link
The powerful LW2760 package is completed by the following comfort factors: Sensor installation only takes a few minutes, and sensor parameters can be conveniently set and read out remotely via IO-Link.