You probably do not come from: Namibia. If necessary, change to:United States
  1. New products
  2. IO-Link
  3. Control module for RGBW LED light bars

Control module for RGBW LED light bars

Create any colour imaginable

This control module for RGBW LED light bars from ifm opens up limitless possibilities in illumination. It enables precise setting of any colour, which is particularly effective when illuminating company logos.

The brightness of the LED light bars can also be adjusted as required to reduce glare when used as a status indicator.

Control via IO-Link or switching signal

Thanks to the integration of IO-Link, it is now possible to define three different display presets, consisting of colour, brightness and flashing pattern, which can be activated either via IO-Link or via the digital inputs on the control module.

The use of IO-Link allows the values for each output to be set individually. This enables a smooth transition between brightness values and colours.