You probably do not come from: Namibia. If necessary, change to:United States
  1. New products
  2. Sensors
  3. The new generation of vortex sensors

The new generation of vortex sensors

Tried-and-tested principle redesigned

New design, improved robustness and proven precision: The new generation of vortex sensors impresses across the board with its internal and external values, making the flow measurement of ultrapure water, water-based media and glycol solutions more straightforward than ever before.

Thanks to the new design and new materials, the number of inner seals could be minimised: housing and bluff body are made of one piece, guaranteeing high pressure and temperature resistance.

More robust against hydrolysis, pressure and temperature

The material used is characterised by high hydrolysis resistance, which has a positive effect on the service life of the device. In addition, the material is resistant to microbiological attack, which reduces the risk of legionella development, especially in cooling water circuits.

Identical installation dimensions

The installation dimensions correspond to those of the existing Vortex generation, allowing for a smooth changeover to the new generation.

Products