You probably do not come from: Namibia. If necessary, change to:United States
  1. New products
  2. Sensors
  3. The SU Puresonic ultrasonic sensor

The SU Puresonic ultrasonic sensor

Ensuring process quality easily and permanently

The SU Puresonic ultrasonic sensor detects flows of conductive and non-conductive media with high precision. Water, glycol mixtures, coolants and oils are all detected with equal reliability.

Robust measuring pipe without structures

The measuring pipe of the SU Puresonic is made of stainless steel and is free of measuring elements, seals and moving parts. This means that faults due to damage, leaks or blockages areexcluded from the outset, as are design-related pressure drops.

Condition monitoring made easy

Equipped with IO-Link and a highly visible status LED, the SU Puresonic has everything you need to continuously monitor process quality. In this way, the status of the signal quality can be quickly read both at the IT level and in the field. If it is decreasing, this can be an indication of increased particle density or deposits on the inner wall of the pipe.

Products