You probably do not come from: Namibia. If necessary, change to:United States

Digital communication to the sensor

  • Precise transmission of process values
  • Less wiring with decentralised IO-Link masters
  • Seamless digital documentation
  • Sensor data can be used in an IIoT context
  • Best possible solution across the entire measuring range:

With IO-Link, the resolution of the conductance is always scaled to suit the used measuring range, so that the highest possible accuracy is guaranteed at all times.

IO-Link converter

The EIO104 converter quickly and easily converts IO-Link process values into two 4...20 mA signals. This means that IO-Link sensors can be easily connected to existing controllers featuring only analogue input cards.

Analogue integration

With analogue integration, the process value is output as a 4...20 mA signal.