You probably do not come from: Namibia. If necessary, change to:United States

High availability in bulk material handling

Monitoring and maintenance
Condition monitoring Availability Machine performance
Case Study

Vibration monitoring on the bucket wheel drive

Transparency

Reduced
set-up times

Increased
machine availability

Results

  • Vibration diagnosis of drive components
  • Maintenance requirements are detected in time
  • Reduction of unplanned downtime
  • High availability

The challenge

Conveyor belts transport the ore to the stockpiles and also back to the cargo ships. For this purpose, so-called stacker-reclaimers or bucket wheel reclaimers are used. The combined stacker and reclaimer equipment picks up the ore with a large bucket wheel rotating above the bulk material. The bucket wheel drive technology is a critical part of these machines. Unplanned breakdowns, which have occurred in the past, sometimes necessitated lengthy repairs.

The reason for this was that there was no possibility of real-time maintenance. In the past, unusual vibrations in the drive technology were detected too late or not at all. The long maintenance times thus had a negative impact on the productivity of the entire system and resulted in high costs. To increase the availability of the bucket wheel reclaimers, the motor and gearbox vibrations were to be monitored in real time to enable an immediate response in the event of an impending fault.

Our customer

Iron ore port

Brazil is the world’s second largest exporter of iron ore. At a port near Rio de Janeiro, even large cargo ships can dock and be loaded with iron ore, which is transported by rail from the country’s mines to the port.

The port has two ore stockpile storage locations with a capacity of 2.5 million tonnes. With a railway siding for unloading wagons and train manoeuvring that is over two kilometres long, bulk material can be transported efficiently.

The terminal has been in operation since 2015, employs around 1,700 people and has a capacity of up to 50 million tonnes of bulk material per year.

Our customer

Iron ore port

Brazil is the world’s second largest exporter of iron ore. At a port near Rio de Janeiro, even large cargo ships can dock and be loaded with iron ore, which is transported by rail from the country’s mines to the port.

The port has two ore stockpile storage locations with a capacity of 2.5 million tonnes. With a railway siding for unloading wagons and train manoeuvring that is over two kilometres long, bulk material can be transported efficiently.

The terminal has been in operation since 2015, employs around 1,700 people and has a capacity of up to 50 million tonnes of bulk material per year.

The solution – why ifm?

The port operator has a long-term cooperation with ifm. Against this background, ifm was able to develop a customised solution based on the requirements right at the start of the project. The reliability and quality of the solution were immediately convincing. Now vibration sensors of the type VSP001 are mounted on the drive technology and the recorded data is evaluated in real time by a VSE151 diagnostic electronics. In addition, sensors of the type TS2229 together with the TP9237 evaluation electronics detect the temperatures at the critical components.

Overall, a very good and transparent picture of the condition of the critical drive components on the machines is provided. As a result, maintenance measures can be better scheduled, avoiding unplanned machine downtimes as far as possible. The overall equipment efficiency is increased by monitoring and diagnosing the machine’s condition. In view of being able to evaluate the vibration diagnosis data even better, the IIoT platform moneo RTM is currently being tested. In this context, also additional systems with inductive or optical sensors are installed. For the future, the port operator expects a considerable reduction in unplanned maintenance measures due to equipment breakdowns.

Case Study: High availability in bulk material handling

These topics might also be interesting for you: