You probably do not come from: Namibia. If necessary, change to:United States

Using sensor technology from ifm for valve control

Other industries
Chemical and process industry
Glass and construction materials industry
Video report

As raw materials are often stored in silos, valve sensors (MVQ) can be used to check whether a valve flap is open or closed – so the first signs of wear can be detected at an early stage. In this way, Sto can also see whether a valve is worn or blocked, which gives them the opportunity to prevent faulty batches and save time and money in production. Another advantage of ifm's sensor technology is the IO-Link connection which allows Sto to access the sensor directly from the central system, making it easy to operate and maintain it.

About Sto

Sto is a manufacturer of paints and plasters, and the world's leading supplier of thermal insulation composite systems, supported by sensor technology from ifm.

About Sto

Sto is a manufacturer of paints and plasters, and the world's leading supplier of thermal insulation composite systems, supported by sensor technology from ifm.

IO-Link systems from ifm

Point-to-point communication with IO-Link systems from ifm

IO-Link has been developed by leading sensor, actuator and control manufacturers. The result is a standardised and fieldbus independent interface for automation. This provides the user with point-to-point connections without complex addressing. Binary switches that used to be limited to simple switching signals or analogue values have developed into smart sensors.

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.