Thanks to innovative PMD technology (PMD: photonic mixer device), the OGD photoelectric distance sensor detects objects with extreme precision up to a range of 2 m.
With this powerful on-chip time-of-flight measurement system, you can detect the presence of objects or their correct installation with maximum accuracy. Typical applications include detection in rapid succession and at high speed, for example in the field of conveying or material handling. The excellent reflection resistance and background suppression of PMD technology, together with a high excess gain, enable reliable detection.
The PMD technology of the OGD sensors is vastly superior to conventional diffuse reflection laser sensors or red light sensors. As their range is angle and colour independent, even difficult objects such as shiny metallic surfaces can be detected.
The reflectivity is output in addition to the distance value. This not only allows identification of objects, but also conclusions about their material properties. Outputting the distance value and reflectivity simultaneously enables material differentiation while also increasing process reliability.
With its M18 thread, the compact laser sensor is easy to install. The setting is made directly on the device or alternatively via IO-Link, using convenient 3-button operation. Visualisation is achieved with the integrated 8-segment 2-colour display on the sensor.
Background suppression is yet another advantage the OGD provides. The feature comes in handy when implementing a stop function at the end of a conveyor belt. Reflections from the metallic rollers do not affect the sensor. The OGD also reliably detects objects of different colours. In this application, the first switch point triggers a speed reduction of the belt. When the object reaches the second switch point, the belt is stopped.
The advantage: By replacing the two devices which are typically required for a light barrier, the OGD helps to reduce the purchase, installation and wiring costs. In addition, it can be used in almost any mounting situation, as it can be aligned to the belt at an oblique angle.
The OGD performs precise and reliable inline quality checks to monitor the correct position and orientation of small shiny components or those with low reflectance such as O-rings or toothed wheels.
Assembly errors such as missing O-rings of 5 mm thickness or more are detected. This error proofing process during production and before final quality checks minimises the risk of costly consequential damage such as plant downtimes or batch failures. At the same time, the inline quality check contributes to long-term and efficient quality assurance. The earlier errors are discovered, the lower the consequential costs are and the sooner improvements can be made.
With increasingly oblique angles, the reflected light diminishes, causing the reflectance value precision to deteriorate.
The OGD reliably detects objects even in unfavourable lighting conditions. It even does not skip reflective materials or those with ragged surfaces such as foils, which often come in colourful or dark designs.
The sensor detects dirt on the lens through the reflectance value via IO-Link and alerts the operator about cleaning. This reduces faulty measurements and increases process reliability.
The ifm distance sensors of the OGD product series use pmd time-of-flight technology for precise, robust and long-range distance measurement. With time-of-flight technology, light waves emitted by the laser light source propagate. When the light bounces off the target, the phase pattern shifts and this shift is directly proportional to the distance.