• Products
  • Industries
  • IIoT & Solutions
  • Service
  • Company
  1. Inclination sensors
  2. Mounting options

Mounting options

Angle and axis definitions as a function of the mounting position

Most inclination sensors available on the market today feature a 3-axis (x/y/z) MEMS accelerometer.
Depending on the sensor type, the final factory calibration determines which measurement axes and also which rotation orientation are used for the respective article. This means that almost any type can be generated from a 3D measuring cell.
Inclination sensors can be mounted horizontally or vertically.
The following pictures illustrate the sense of orientation and rotation as a function of the mounting position.

Horizontal mounting of 1-axis inclination sensors

If the sensor is mounted horizontally, it can map a rotation around its x- or y-axis:

Vertical mounting of 1-axis inclination sensors

If the sensor is mounted vertically, only a rotation around the z-axis makes sense for a 1-axis sensor:

Horizontal mounting of 2-axis inclination sensors

If a 2-axis sensor is mounted horizontally, it can map a rotation around its x- AND y-axis:

Vertical mounting of 2-axis inclination sensors

In vertical position, the 2-axis sensor can also output x- AND y-angles: