The Vision Assistant offers 5applications: depalletising, robot gripper navigation, completeness monitoring, object dimensioning and level. A wizard guides the user through the application settings. This is self-explanatory and intuitive. The requested application can be set up and started in just a few minutes. The predefined applications make it possible to implement automation solutions, but the Vision Assistant can do more: In the extended parameter setting mode,experienced users can extend the given applications or create their own application solutions.
Constant exchange with users and extensive handling tests have led to an extraordinary simplification of sensor handling and integration.
At the same time, accuracy is still guaranteed and individual adjustments are still possible. Individual adaptation to the environment leads step by step to the required application.
Applications - out of the box
Installing the 3D sensor is easy thanks to the guiding wizard for the following applications
Customisation or extension of applications
Application example distance measurement on an AGV or lift truck
The O3D camera and the software development kit can be used to develop individual solutions and applications.
If the camera is integrated into a machine, the measured data can be evaluated with common image processing libraries. A software development kit with code samples is available in different programming languages.