You probably do not come from: Germany. If necessary, change to:United States
  1. The Y path
  2. Energy Monitoring

Energy Monitoring with the Y path from ifm

Energy consumption and the resulting cost are the main factors which are decisive for an efficient production. Only if you monitor these values continuously and lastingly you will be able to correctly assess and take futures measures to reduce energy consumption.

Make use of the possibilities:

  • Consumption data for energy optimisation: relationship between pressure, consumption and speed in the cockpit of the LINERECORDER SMART OBSERVER
  • Order-related consumption data with time stamp for SAP evaluations
  • Control of the valves and feedback of the end positions via all important fieldbuses
  • Local display for the configuration of the IT connection
  • Counter for machine cycles and switching operations of valves
  • Flexible extension
  • Local data buffering with time stamp

LINERECORDER SMART OBSERVER software

The SMART OBSERVER software from ifm is used for condition monitoring of systems and the observation of the energy consumption. Versatile evaluation options in conjunction with corresponding alarm scenarios are available for the analysis of the situation:

  • Current status indications
  • Parallel indication of comparative values from the past
  • Analysis of different time ranges
  • Observation of several process values in the same time range
  • Correlation of several states
  • Easy organisation of favourites
  • Alarm management

Online Monitoring

Irrespective of location and time users have access to all acquired data, analyses and alarms. All web-based information and functionalities from the manufacturing environment can be securely accessed and processed worldwide and the user is immediately informed about incidents by text message or e-mail.

LINERECORDER SMART OBSERVER

ENERGY MANAGEMENT AS IN THE CASE OF THE COMPANY RAMAPLAST

Application example: Energy Monitoring.