- From vibration monitoring to Industry 4.0
- More information
More information about vibration monitoring
Brochures:
![](/responsive/medium/fourbythree/content/gallery/microsites/schwingungsueberwachung/ifm-schwingungsueberwachung-cover-en20.png?v=542526481)
From vibration monitoring to Industry 4.0
Automatic plant protection - Permanent vibration diagnostics in mineral water bottling
The wear of machine parts cannot be prevented. Permanent vibration diagnostics, however, ensures that such damage is reliably detected in time. Hassia-Mineralquellen, one of Germany's largest mineral springs, rely on permanent electronic vibration diagnostics from ifm in bottle filling. The investment already paid off in the pilot phase: Imminent damage to a drive was detected in time and eliminated. Unplanned downtime could thus be prevented.