Using the Network Scan Feature in Moneo Configure
If I click on the specific IP address button and enter the known IP address of the IO link master that I am looking for and press scan, it will do the same thing where it will begin to search for it.
And you can see the search for search bar across the top begin to load. So once the scan is complete, again, you can see done at the bottom of the page, you can see it has found that AL1322 IO link master with the IP address that I entered and it will show you any devices connected to that IO link master.
For example, I have a TA2603 temperature sensor connected on port one. So now finally, if I go back into the network scan button, you will see there is a scan all button.
If you click on this and then press scan, it will begin looking for any devices you have connected on the network.
Now you can see it is searching and it has found the programing cable and the TD temperature sensor as well as the IO link master that I have connected on the network.
So there you have it. That concludes this Tech Insights video on scanning your network in the moneo configure software. A
s always, you can check out our Learn More section on our website for helpful information on any of our products.
Feel free to contact us at info.us@ifm.com or call into 1 800 441 8246 to speak with somebody who can assist you.
Thank you for your time and have a great day.
Learn more about activating Moneo software, the Read and Write functions on Moneo software or changing the IP address for a Moneo system.