You probably do not come from: Namibia. If necessary, change to:United States
  1. moneo IIoT platform
  2. Guidance and support
  3. How-to videos

How-to videos

To make it even easier for you to get started and use moneo, we provide you with our own how-to videos. Our product managers not only explain and demonstrate the most important steps in the moneo software but also answer questions clearly – for example, how to make your data from moneo available via OPC UA server or how to download configure free.

It is possible that the cloud subscription is not yet available in your region.

Take a look and be inspired by our solutions!​

 

Security

RTM

edgeConnect

configure

Industrial AI Assistant

moneo Cloud

Set up the moneo Cloud instance

Learn how to create a user in the mobile IoT suite, have your licence activation code ready.

 

Set up moneo edgeGateway and connect it to the moneo Cloud

Find out how to carry out the initial set-up and connect the moneo edgeGateway to your Cloud instance.

 

Using the moneo Cloud

Get to know the first steps in the moneo Cloud.

Security

How can I access moneo from a remote system?

Changing the host name in a Windows system

In our how-to video, Matthias Schmidt, Product Manager moneo, shows you how to change your access to moneo from your local address in just a few minutes, allowing you also to access moneo from remote systems.All that is required is to change the host name in a Windows system.

Watch the video and find out how fast and simple it can be!

How do I encrypt my moneo data?

Activating TLS transport encryption in a Windows system

Would you like to enhance the security of your moneo data even more? In our how-to video, Matthias Schmidt, Product Manager moneo, shows you how to enable encrypted communication in moneo.

moneo offers http access as standard, but you can quickly and easily switch to the secure https protocol.

How do I back up my moneo data?

Automatic back-up via Windows Task Scheduler

Would you like to protect your moneo data? In our how-to video, Matthias Schmidt, Product Manager moneo, shows you how to activate the protection back-up script.

Backing up your data allows you to restore the settings of your moneo instance in minimum time should a system defect or configuration issue occur.

RTM

Monitoring vibration sensors with moneo

Advanced Vibration Analysis

How can I set up the AVA wizard in moneo?

In this video, Nikolaj Setzkorn, Product Manager moneo RTM, shows you how to set up fan vibration monitoring in moneo within a few minutes using the AVA wizard – a five-step set-up wizard. Once you have successfully onboarded the devices, you can create a new dashboard. Use the AVA wizard to define new threshold values quickly and easily.

This allows you to create warnings and alarms and be informed of deviations in the future.

edgeConnect

How do I connect my moneo system to the Microsoft Azure IoT Cloud?

Simply connected: Microsoft Azure IoT Hub Connector

Would you like to transfer your data from moneo to the cloud and process it there?

In our how-to video, Matthias Betz, Product Manager moneo edgeConnect, shows you how you can connect the cloud connector to your moneo system to get even more benefit from your data in the future.

The video shows you how quick and easy it can be!

How do I connect my moneo system to the AWS IoT Core Connector to transfer data to the cloud?

Simply connected: Amazon Web Services (AWS) IoT Core Connector

Would you like to push your data from moneo to the cloud and process it there?

In our how-to video, Matthias Betz, Product Manager moneo edgeConnect, shows you how to connect your moneo system to the AWS IoT Core Connector and activate data exchange in the cloud.

Very quickly and simply!

How do I make my data from moneo available via OPC UA server?

Simply connected: OPC UA server

Would you like to make your data from moneo available to other systems via an OPC UA server?

In our how-to video, Matthias Betz, Product Manager moneo edgeConnect, shows you how to transfer your information via OPC UA server, establish a connection to an external OPC UA client and make your data available to a third-party system.

Take a look now and discover the possibilities!

configure

How do I install moneo configure free and how do I use the software for parameter setting?

moneo configure free: Free installation and set-up

Are you looking for an intelligent solution to set the parameters of your IO-Link devices?

In our how-to video, Kai Bürger, Product Manager moneo configure, shows you how you can easily install the free version of our parameter-setting software on your computer and start parameter setting immediately!

Integration of IO-Link device parameters into GSDML

Simple GSDML parameter setting of ifm IO-Link master gateways (Al14xx and AL1304-07) with moneo configure PLC Tools.

User-friendly: one tool for all IO-Link devices and the automated transfer of the settings in case of device replacement will reduce the workload thanks to your predefined files.

Clearly structured: take advantage of the clearly structured user interface of moneo configure and access the IO-Link device parameters directly in the TIA Portal as well.

Industrial AI Assistant

Walkthrough: moneo SmartLimitWatcher

Walkthrough: moneo PatternMonitor