- SA flow sensor
- Setup and support
- Installation guidelines
Installation guidelines for the SA flow sensor
For best performance of the SA family of sensors, please adhere to the following guidelines. Should you need additional support, feel free to contact our service center at 888-704-0702 and speak to one of our applications engineers.
Insertion depth
As seen in the Technology section, the SA sensor monitors the difference in temperature of two RTDs - one located at the tip that reacts as the flowing medium conducts heat away and one located ~15 mm above that provides the medium reference temperature.

To accurately account for any medium temperature changes, the tip of the sensor must be located within the flowing medium. The SA4 series offer sensors with 100 mm or 200 mm probe lengths used with compression fittings for adequate insertion depth in larger pipe sizes.

Minimum insertion depth based on pipe diameter
Note: For very viscous or high-velocity media that exerts a strong bending force on the probe, the above insertion depth should not be exceeded.
Pipe mounting
To help ensure the sensor tip is surrounded by the medium, always mount the sensor in a vertical section of pipe with flow going up. This method guarantees the pipe is full. If horizontal mounting is the only option, mount at an angle in case the pipe may not be full.

Recommended mounting
If the pipe is guaranteed to be full, the sensor may be mounted from the top.
Because of the principle of operation, build-up on the sensor tip affects heat conduction. If the medium is free from build-up, horiztonal mounting from the bottom is possible.
Be sure to thoroughly test the sensor in these situations.

Conditional mounting
Two mounting situations that are not recommended in any case are:
- Sensor tip in contact with the opposite pipe wall. This will adversely affect the heat conduction process.
- In a pipe with downward flow that is open to atmosphere and not a closed loop system. The velocity profile in such a situation is not repeatable.

Not recommended
Straight pipe run
The SA sensor is the most reliable and repeatable when the sensor is installed in laminar flow. Valves, bends, flow constrictions, etc. all cause turbulence.
To avoid influences of turbulence, maintain a straight run of 5...10 x pipe diameter upstream of the sensor and 3...5 x pipe diameter after the sensor.

D = pipe diameter, S = source of turbulence
Alignment
The SA sensors either have a dimple on the mounting nut (on units with threads) or a large and small wrench flat (for units requiring compression fittings). The dimple and large flat indicate the side of the probe where the reference RTD is located. For best response to change in medium temperature, install the sensor with the flow hitting this reference side first.
If necessary to read the display, the sensor housing can be rotated up to 345°.

1 = wrench flats, 2 = dimple