• Products
  • Industries
  • IIoT & Solutions
  • Supply Chain Software
  • Service
  • Company
  1. moneo IIoT platform
  2. Products
  3. moneo Industrial AI Assistant
  4. PatternMonitor

moneo PatternMonitor

Detecting unwanted changes in critical process values

moneo PatternMonitor is a smart, innovative AI-based solution that monitors stationary and continuous processes. It identifies structural changes. In the event of anomalies in individual critical process parameters such as temperature, flow and vibration, appropriate measures can be triggered through an early alarm.

Benefits of moneo PatternMonitor

Simple
No data science expertise required. Pragmatic solution with simple 5-step wizard for those responsible for production and maintenance.

Convenient
Automated data preparation, quality checking and parameter setting for pattern detection.

Smart
Automated detection of structural changes in the critical process variable using AI methods.

Reliable
Continuous background monitoring and alarming when patterns change.

Customisable
Adjustable sensitivity for detecting patterns and anomalies in the evaluation period.

Detect changes quickly with the 5-step wizard

moneo PatternMonitor offers a set-up wizard that makes the software easy to use. In just five steps, the intelligent monitoring tool can be activated without expert support.

moneo Pattern Monitor identifies structural changes in critical process values. Automatically generated alarms enable appropriate measures to be initiated at an early stage.

Customers who prefer to monitor a range of dynamic processes can use moneo SmartLimitWatcher. The software automatically detects anomalies based on sensor data such as temperature, flow and vibration and sends warnings and alarms based on dynamic thresholds.

➜ Learn more about moneo SmartLimitWatcher

By the way:
further intelligent tools in the area of predictive maintenance are already in development and will soon be added to the existing Industrial AI Assistant solutions.